Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Dear TI Support Team,
I am using the CCS v7.0.0.00042 and since the latest update of the TI-Emupack 6.0.579.0 I have some trouble during the linking of my DSP software.
After starting of CCS, I can compile and link my application.
After running the software on the target board, the software is not linkable anymore. The linker stops with error:
<Linking>
fatal error #10296: cannot open output file "...xyz.out" for writing
>> Compilation failure
In addition, it look so that the ccstudio.exe leaves open the output file multiple time after starting the debug session.
The closing of debug session does not help. I have to close and restart the CCS, if I want to recompile my application.
Do you have any idea, what is going wrong?
Thanks and kind regards
Sven