Hi,
I was hoping to find a command-line solution that can flash a CC13xx natively on Linux. So I installed UniFlash 4.1.1.1241 on a machine running Xubuntu 16.04 (64 Bit). I selected CC1310_LAUNCHXL as a board and clicked on the Start button. Then I get this error message:
[3339:0319/183704:INFO:CONSOLE(446)] ""2017-03-19T17:37:04.700Z" "ERROR" "DAEMON" "cloud-agent-server" "/opt/ti/uniflash_4.1/ticloudagent/server/common/generate_error_handler.js:9:16:()" "[\n {\n \"requestId\": undefined,\n \"error\": {\n \"type\": \"Error\",\n \"message\": \"EACCES, open '../deskdb/content/TICloudAgent/linux/ccs_base/common/targetdb/connections/TIXDS110_Connection.xml'\",\n \"stack\": [\n { name: \"Error\", loc: \"native\" }\n ],\n \"errno\": -13,\n \"code\": \"EACCES\",\n \"path\": \"../deskdb/content/TICloudAgent/linux/ccs_base/common/targetdb/connections/TIXDS110_Connection.xml\"\n }\n }\n]"", source: /opt/ti/uniflash_4.1/dinfra-library/desktop/dlog.js (446) [3339:0319/183704:INFO:CONSOLE(536)] ""log flushes failing;" "will message again on success"", source: /opt/ti/uniflash_4.1/dinfra-library/desktop/dlog.js (536)
Nothing happens after that. What do these error messages mean?