Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
I created empty project with main() for CC13x0f128 but I got unresolved symbol ResetISR from cc130x0128.cmd file ?
Project failed to link. I have CCv7 .
I removed --entry_ponit ResetISR line from linker file but after successful link and download CC1310 got locked so I cannot load code any more.
First time I load project loads and runs immediately with no jump to main and no run button .
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Second time I try load I get this error.
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target to halt
Cortex_M3_0: GEL: File: C:\Users\arudel\workspace_v7\Boot\Debug\Boot.out: Load failed.