Tool/software: Code Composer Studio
Hi,
I have two boards connected to my PC through JTAG connector. One is
- TMS320-JTAG-USB for this connection in Target configuration file under the connection type I am selecting Texas Instruments XDS100v2 USB Debug probe.
- Spectrum Digital xds200- For this connection in Target configuration file under the connection type I have selected Texas instruments XDS2xx USB Debug probe.
When I open the target configuration file in Code composer studio and click on test connection for each of the connection, I am successfully getting this message.
The JTAG DR Integrity scan-test has succeeded.
I wanted to automate this task, so i just run the below command from the uscif folder in cmd.
dbgjtag.exe -f C:\Users\AppData\Local\TEXASI~1\CCS\ti\0\0\BrdDat\testBoard.dat -S integrity -rvtestBoard.dat -S integrity -rv
But this doesn't work for two JTAG Debug probe. By default it will run xds200.0ut and gives the value that its integrity scan test has succeeded. I wanted for both the JTAG Debug probe scan test to be done .
Kindly let me know is there any way to do test condition when more than two boards are connected by using different JTAG Debug probe by using dbgjtag.exe application.
Regards,
Dhanya