Hello,
I'm trying to build some sample applications with GUI composer to interface with MSP430. I created a simple dashboard with a Meter component, then run the File->Export->As Stand-Alone App. The GUI Composer Runtime is already installed. Most of the times I only get the Export dialog box (see below) that takes forever without any result (this is the general issue).
- Windows GUI Composer Runtime Installer: Download
- Linux GUI Composer Runtime Installer: Download
- OSX GUI Composer Runtime Installer: Download
(For detailed instructions, please click the Help icon in the upper right corner)
Processing...
Few times I got the zip file, installed it in the guicomposer runtime folder and run the win32_start.bat. It fails calling the win32_splash.bat file, since there is no file with this name in the splash folder.
Thanks for any suggestion
Fabio