Tool/software: Code Composer Studio
Hi there,
I ran into this weird problem when trying to build a ccsv6 project. This project was converted from ccsv3.3 to ccsv6. After fixing some of the immigration problems, Build Project gives me 60+errors, basically saying symbols not resolved. Then I check back, I find that some of the files in the source file folder are not built at all. Meanwhile the others are successfully built.
Things I have checked:
1. These files are NOT set to exclude from building.
2. In project properties, I can see they ARE in the linked resources. Also I can see the small arrowhead on the bottom right corner of the file icon in project explorer. I tried both linked them and copy to workspace. No luck.
3.There are no other file saying those files should be skipped from building.
Some observations:
1. Those skipped files are not shown in the projectname_linkInfo.xml, either in makefile. But I have no idea why they are excluded.
2. All the files that are skipped appear to have all upper case letter names in the file system, but in linked resource settings, they are of lower cases. I tried to modify the names to be the exactly the same, still no luck.
I have run out of options to try... Any ideas what should I do?