Tool/software: Code Composer Studio
Hello,
I can unlock the micro using C2Prog.exe; however, after the micro is locked, I am not able to connect to the target using the XDS100v2 debugger.
According to SPRU963A (Page 23), there are two ways to connect an emulator (e.g. XDS100v2) to the target after the target has been locked:
1. Use the use the “Branch to check boot mode” boot option.
My hardware doesn't have the switches to set the Branch to check boot mode” boot option.
2. Use the Wait-In-Reset emulation mode.
I set EMU1 to high and EMU0 to low in the Advanced Target Configuration (see Below) and programmed the device with a password other than all ones . After doing so and resetting the device, I am still not able to connect (see connection error dialog box below).
What am I doing wrong?
Stephen