This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Known Issue: CCS on Linux crashing on startup

Guru**** 420930 points
Other Parts Discussed in Thread: CCSTUDIO

Tool/software: Code Composer Studio

There is a known issue with CCS on Linux crashing on startup (segmentation fault). This issue occurs after updating the Linux environment with the latest available packages. This issue is under investigation.

Sorry for the inconvenience

Thanks

ki

UPDATE 1: Please use the workaround in the post below:

https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/604599/2226461#2226461

This addresses both the CCS startup issue and the xdc build failure

UPDATE 2: The latest Linux update has a fix for this issue. This was confirmed in Ubuntu 16.04 (kernel 4.4.0-83.106)

  • Tracking ID for this bug is: CCDSK-2703
  • Glad to see others with the same problem. How can I help investigate this?
    I also posted this before: e2e.ti.com/.../604596
  • Thanks, didnt see it when I looked up possible error, probably didnt use correct keyword..
    Working fine from ./eclipse
  • Here's a workaround for the issue while we figure out the root cause.

    Open  <install dir>/ti/eclipse/ccstudio.ini in a text editor.  Comment out the first two lines by inserting a # at the start of the line. It would look like this:

    #-vm
    #jre/lib/amd64/server/libjvm.so

  • I've noticed one side effect of making this edit - I cannot import any CCS projects into the current workspace. Weird.
    <shrug>
  • Although the quick fix (removing the -vm) worked for starting CCS, I also see an (probably related) issue with the XDCtools:

    A SYS/BIOS project (for C6678 DSP) that compiled before does not build anymore. Same thing when I create a fresh "Typical" SYS/BIOS Template it does not build either:

    **** Build of configuration Debug for project gfaulttest2 ****

    /localdata/home/me/ti/ccsv7/utils/bin/gmake -k -j 12 all -O
    gmake[1]: Entering directory '/localdata/home/me/repositories/BP_GPUDSP/ti_ccs/gfaulttest2/Debug'
    Building file: ../app.cfg
    Invoking: XDCtools
    "/localdata/home/me/ti/xdctools_3_32_02_25_core/xs" --xdcpath="/localdata/home/me/ti/bios_6_46_04_53/packages;/localdata/home/me/ti/openmp_dsp_c667x_2_06_00_00/packages;/localdata/home/me/ti/ctoolslib_2_2_0_0/packages;/localdata/home/me/ti/edma3_lld_2_12_03_27/packages;/localdata/home/me/ti/framework_components_3_40_02_07/packages;/localdata/home/me/ti/framework_components_3_40_02_07/examples;/localdata/home/me/ti/pdk_c667x_2_0_5/packages;/localdata/home/me/ti/ccsv7/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.platforms.evm6678 -r release -c "/localdata/home/me/ti/ti-cgt-c6000_8.1.3" --compileOptions "-g --optimize_with_debug" "../app.cfg"
    subdir_rules.mk:10: recipe for target 'build-1863261585-inproc' failed
    gmake[1]: *** [build-1863261585-inproc] Segmentation fault (core dumped)
    gmake: *** No rule to make target 'build-1863261585', needed by 'configPkg/compiler.opt'.
    gmake[1]: Leaving directory '/localdata/home/me/repositories/BP_GPUDSP/ti_ccs/gfaulttest2/Debug'
    gmake: Target 'all' not remade because of errors.

    **** Build Finished ****

    I also tried installing oracle JVM 1.8.0_131 as default instead of OpenJDK 7 with no luck.
    The XDCtools 3.50.2.20_core show the same issue, too.
    My system is Linux 3.13.0-121-generic #170-Ubuntu SMP Wed Jun 14 09:04:33 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux.

  • My workaround is to bypass ccstudio and just run the eclipse directly, so far all is correct, but interface a little different.

     <install dir>/ti/eclipse/  ./eclipse

  • I have the same issue. With the quick fix I can start CCS again but I cannot compile anymore due to the XS segmentation fault.

    Looking at the XS script it is using LD_LIBRARY_PATH="${ROOT}:${ROOT}/jre/lib/amd64/server:${ROOT}/jre/lib/amd64$_cur"

    My system: 4.8.0-56-generic #61~16.04.1-Ubuntu SMP Wed Jun 14 11:58:22 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux

  • If you keep older kernels you can grub into a version previous to the linux-firmware update. This is my current work-around to be able to compile.
  • Hi, Mr. Lee!
    Do you have an update in this issue?
  • Hello all,

    The issue appears to be related to:

    https://bugs.launchpad.net/ubuntu/+source/linux/+bug/1699772

    askubuntu.com/.../eclipse-crashes-with-linux-kernel-4-4-0-81-generic

    The workaround mentioned there seems to also apply to CCS:

    Open terminal

    $ export JAVA_TOOL_OPTIONS=-Xss1280k

    then, from the same terminal, launch the ccstudio application in . /ccsv7/eclipse

    This should help with both CCS startup and the xs build issues.

    NOTE: On some systems, this is enough to start CCS, but not enough to avoid the build error. In those cases, increase the max stack size to 2650k (ex: export JAVA_TOOL_OPTIONS=-Xss2560k)

    This workaround does not need the modification to the ini file mentioned earlier (commenting out the first two lines). A stock ccstudio.ini file can be used with the workaround above.

    We are still investigating. Sorry for all the inconvenience.

    ki

  • This is really holding me back, how soon will it be fixed?
  • Silver Diamond said:
    This is really holding me back, how soon will it be fixed?

    Did you try the workaround in the post prior to yours?

    Thanks

    ki

  • Ki,

    the workaround solves the issue for me, thank you very much!

    Clarification on the instructions, just in case:
    After the export JAVA_TOOL_OPTIONS=-Xss1280k you need to stay in that terminal, cd your way to your CCS installation,
    in my case cd ~/ti/ccsv7/eclipse and run ./ccstudio
    I recommend not putting it into your .bashrc or similar at this point, since not all eclipse IDEs are impacted (e.g. my Nsight 8.0 runs fine).


    -----

    Confirmed with both project I posted about earlier (using xdctools_3_32_02_25_core and ti-cgt-c6000-8.1.3) on:
    Linux 3.13.0-121-generic #170-Ubuntu SMP Wed Jun 14 09:04:33 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux
    System java -version: Java(TM) SE Runtime Environment (build 1.8.0_131-b11)

  • Faced the same problem with segfault in xdctools today after Ubuntu update.

    Have to uninstall kernek update:

    sudo apt-get remove linux-image-4.8.0-56-generic linux-image-extra-4.8.0-56-generic 

  • ChrisF said:
    Clarification on the instructions, just in case:
    After the export JAVA_TOOL_OPTIONS=-Xss1280k you need to stay in that terminal, cd your way to your CCS installation,
    in my case cd ~/ti/ccsv7/eclipse and run ./ccstudio
    I recommend not putting it into your .bashrc or similar at this point, since not all eclipse IDEs are impacted (e.g. my Nsight 8.0 runs fine).

    Thanks for the clarification. Yes, you need to run everything from the same terminal.


    Note that this issue was cause by a security fix in the kernal. A new version of the fix that does not cause the issue is being tested and I anticipate will be released soon. So hopefully this workaround will not be needed for long

    Thanks

    ki

  • Ki,

    This workaround also worked for me.

    The only issue was that, even after export the variable and been able to run ccstudio, the Xs compiler still crashed with the Segmentation Fault error.

    The solution was to change the value of the exported variable from "JAVA_TOOL_OPTIONS=-Xss1280k" to "JAVA_TOOL_OPTIONS=-Xss2560k".

    Do you see any problem with this solution?

    Also, to make life easier, I created a bash script in <install folder>/ccsv7/eclipse with name ccstudio.sh where I export the variable and then execute ccstudio. To use it, I just changed the Exec= parameter of the desktop launcher, pointing to this script. This way I can keep using the desktop icon to start the application.


    Thanks.

    Cassiano.
  • In the past couple days two of our engineers have been unable to build Vision SDK projects and we suspect it is this issue as well. They are both using Ubuntu 16.04 and had CCS7 installed on their PCs.

    /home/linuser/Documents/sdks/tda3/sdk_manager/staging/vision_sdk/binaries/maketemp_configuro_cmd_ipu1_1.bat: line 1: 22759 Segmentation fault      (core dumped) /home/linuser/Documents/sdks/tda3/sdk_manager/staging/vision_sdk/../ti_components/os_tools/linux/xdctools_3_32_00_06_core/xs xdc.tools.configuro --generationOnly -o /home/linuser/Documents/sdks/tda3/sdk_manager/staging/vision_sdk/binaries/obj/vision_sdk/tda3xx-rvp/ipu1_1/release/vision_sdk_configuro -t ti.targets.arm.elf.M4 -p ti.platforms.evmTDA3XX:IPU_1_1 -r release -b /home/linuser/Documents/sdks/tda3/sdk_manager/staging/vision_sdk/build/tda3xx/config_m4.bld --cfgArgs "{mode: \"\", coreName: \"IPU1-CORE1\",  platformMem: \"DDR_MEM_512M\"}" MAIN_APP_ipu1_1.cfg

    In this case the build on the machine was working one day and stopped the next, even when a fresh checkout of the codebase was completed.

  • Same here. After recent Ubuntu 16.04 updates were installed, CCS v7.1 crashed immediately after the launch. Today I noticed that xds also crashed due to segfault, and no longer able to build even though the source code was not modified at all.

     

  • I have same issue after applying the quick ccs fix. Using 4.10.0-24-generic #28-Ubuntu SMP Wed Jun 14 08:14:34 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux
  • On my Ubuntu machine (4.4.0-81-generic #104-Ubuntu SMP x86_64 GNU/Linux), which I just updated, CCS 7.1 stopped working as well.

    So, I added this line '-Xss1280k' into ccstudio.ini and everything seems OK so far.
  • Modifying ccstudio.ini will allow you to start up CCS but you will run into build issues if you are using TI-RTOS. Hence the environment variable workaround is recommended:
    e2e.ti.com/.../2226461

    Thanks
    ki
  • You are right..... thanks.

    But, it doesn't compile completely as you can see here...

    **************************************************************************************

    # making package.mak (because of package.bld) ...

    ...

    #
    # making package.mak (because of package.bld) ...
    ...

    subdir_rules.mk:24: recipe for target 'build-326279697-inproc' failed
    Picked up JAVA_TOOL_OPTIONS: -Xss1280k
    Picked up JAVA_TOOL_OPTIONS: -Xss1280k
    gmake: *** Deleting file `package.mak'
    Picked up JAVA_TOOL_OPTIONS: -Xss1280k
    gmake: *** Deleting file `package.mak'
    gmake: *** No rule to make target `.configuro'.  Stop.
    js: "/home/ybonin/ti/xdctools_3_32_01_22_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
    gmake[1]: *** [build-326279697-inproc] Error 1
    gmake: *** [build-326279697] Error 2
    **************************************************************************************

    Any clue ???

  • Good, however on linux Kernel 4.10.0-24-generic (Ubuntu 17.04) I also had to comment 2 lines on the top of the ccstudio.ini file to make it work.

    It will be nice to have this info added back on TI wiki. http://processors.wiki.ti.com/index.php/Download_CCS


    #-vm #jre/lib/amd64/server/libjvm.so

  • Yves - try increasing the max stack value more like mentioned in the below post:
    e2e.ti.com/.../2227526
  • It works fine with -Xss2560k

    Thanks.
  • Hello,

    We had the problem with Likux Kernel 3.13.0-121 so we downgrade it until found a combination of Lunix Kernel-CCS that works.


    These are the versions:

    • Linux ialbar 3.13.0-119-generic #166-Ubuntu SMP Wed May 3 12:18:55 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux
    • CCS v5.5 and CCS v6.2.

    We hope that this information will be helpful to someone.

    Best regards.

  • This workaround doesn't work for me.

    Would it be possible to get more information about the problem and how it's affecting CCS/xdc?

    Thank you

  • The workaround JAVA_TOOL_OPTIONS= -Xss2560k has been working for me. It fixed both CCS and XDC issues.

  • Annette Keller said:

    This workaround doesn't work for me.

    Would it be possible to get more information about the problem and how it's affecting CCS/xdc?

    Hi,

    I am not sure if that is your case, but I needed to run my CCS as sudo and was unable to apply the workaround. In this case, before I set the Java options I started a persistent sudo subshell. In other words:

    user@host:~$ cd /opt/ti/ccsv7/eclipse
    user@host:/opt/ti/ccsv7/eclipse$ sudo -i
    user@host:/opt/ti/ccsv7/eclipse# set JAVA_TOOL_OPTIONS=-Xss2560k
    user@host:/opt/ti/ccsv7/eclipse# ./ccstudio &

    By the way, when running as sudo the -Xss1280 issued segfaults for me.

    Hope this helps,

    Rafael 

  • In our case, some of CCS tools weren’t working, for example, tcf configuration tool couldn’t start.
    CCS was able to compile and load program.

    Paloma
  • Hello,
    A update that fixes the issue has been released for several platforms. Please check for available updates. This was confirmed in Ubuntu 16.04 (kernel 4.4.0-83.106)

    Thanks
    ki
  • Hi,

    I can attest that updating my Ubuntu 16.04/64 with today's kernel patches is enough to allow CCS to be properly launched. The packages installed today were:

    Linux said:

    user@host:~$ ls -lt /var/lib/dpkg/info

    -rw-r--r-- 1 root root 1510 Jun 29 09:05 nautilus.list
    -rw-r--r-- 1 root root 728 Jun 29 09:05 nautilus-data.list
    -rw-r--r-- 1 root root 198 Jun 29 09:05 linux-headers-generic-hwe-16.04.list
    -rw-r--r-- 1 root root 716176 Jun 29 09:05 linux-headers-4.8.0-58-generic.list
    -rw-r--r-- 1 root root 1093378 Jun 29 09:05 linux-headers-4.8.0-58.list
    -rw-r--r-- 1 root root 192 Jun 29 09:05 linux-image-generic-hwe-16.04.list
    -rw-r--r-- 1 root root 174 Jun 29 09:05 linux-generic-hwe-16.04.list
    -rw-r--r-- 1 root root 330340 Jun 29 09:05 linux-image-extra-4.8.0-58-generic.list
    -rw-r--r-- 1 root root 80015 Jun 29 09:05 linux-image-4.8.0-58-generic.list
    -rw-r--r-- 1 root root 515 Jun 29 09:05 libnautilus-extension1a:amd64.list
    (...)

    My kernel is still 4.8.0-58

    Linux said:

    user@host:~$ uname -a
    Linux host 4.8.0-58-generic #63~16.04.1-Ubuntu SMP Mon Jun 26 18:08:51 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux

    Regards,

    Rafael

  • I am getting a similar behavior, but I am not sure it is the same thing. I ran updates on a build machine yesterday that has been building ccs projects for a very long time. Today I get segfault with ccs and eclipse. I am running CCS 6.1...

    There was a linux kernel update, but this is definately not as new as the report above.
    Environment is Ubuntu 14.04
    uname -a
    Linux 3.13.0-128-generic #177-Ubuntu SMP Tue Aug 8 11:40:23 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux

    I tried the workaround with no success
    ./ccstudio
    Picked up JAVA_TOOL_OPTIONS: -Xss2560k
    Segmentation fault (core dumped)

    gdb output:
    Starting program: /home/parallels/ti/ccsv6/eclipse/ccstudio
    [Thread debugging using libthread_db enabled]
    Using host libthread_db library "/lib/x86_64-linux-gnu/libthread_db.so.1".
    process 14231 is executing new program: /home/parallels/ti/ccsv6/eclipse/ccstudio
    [Thread debugging using libthread_db enabled]
    Using host libthread_db library "/lib/x86_64-linux-gnu/libthread_db.so.1".
    Picked up JAVA_TOOL_OPTIONS: -Xss2560k

    Program received signal SIGSEGV, Segmentation fault.
    0xf628d15b in _expand_stack_to(unsigned char*) ()
    from /home/parallels/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
  • Ryan, I believe your linux version is affected by the bug. If there is not a later update with the fix, then you can try rolling back to linux-image-3.13.0-119-generic. That is the last known good version

    Thanks
    ki