Other Parts Discussed in Thread: CC3200
Tool/software: Code Composer Studio
Because I'm using a LP board to test my application I bought an XDS110 (TMDSEMU110-U) to program and debug my custom board.
After connecting the debugger to the PC (Windows 10) it installed the related drivers, also for the two CDC UART ports.
The user/application UART does not work: I monitor the pin UARTTX on the auxiliary connector but it is at 0V level. I expect a logic high on idle. Even opening the port in a serial terminal and send something changes nothing.
Do I need to set something in order to enable this UART?