Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hello,
I am trying to use the CCS Cloud and it seems to lack some features that enable RF development. Information can be found below.
- CCS Cloud 1.6.0
- Windows 10 Professional, 64 bit
- FireFox 54.0.1 (64-bit)
- Session ID: 1498754303653_00000535
- TI LAUNCHXL-CC1310
Imported projects from TI Resource Explorer Works compile flawless. Generating new projects for the LAUNCHXL (using XDS110 USB Debug Probe) cannot be compiled with RF settings generated by SmartRF Studio. Comparing the Compile commands from imported and generated projects there are some includes missing. And the command lines (Project properties -> Build -> ARM Compiler) cannot be edited.
Imported projects compile command line:
-mv7M3 --code_state=16 --float_support=vfplib -me --include_path="@workspace/rfPacketRx_CC1310_LAUNCHXL_nortos_ccs" --include_path="@ti-rex-content/simplelink_cc13x0_sdk_1_40_00_10/source" --include_path="@ti-rex-content/simplelink_cc13x0_sdk_1_40_00_10/kernel/nortos" --include_path="@ti-rex-content/simplelink_cc13x0_sdk_1_40_00_10/kernel/nortos/posix" --include_path="@ccs/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" --define=DeviceFamily_CC13X0 -g --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on
Generated projects compile command line:
-mv7M3 --code_state=16 -me --include_path="@workspace/ZenOne" --include_path="@ccs/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi
Is there a way to add include paths to the compile command line? Or at least chose the libraries to be included?