Tool/software: Code Composer Studio
I've loaded code composer studio version 6 onto 3 different computers now, the latest running Windows 10, and I still can't connect to the USB JTAG on the C5517 EVM. I need CCSv6 for this particular demo.
The problem is always the same. The USB driver seems ok and is the right version (according to one e2e post). The windows device manager shows the "Spectrum Digital TMS320C5517 DSK" device driver which is at version 6.0.999.2. The Spectrum Digital DSK-EVM-eZdsp onboard USB emulator connection appears in CCS, but the test button is greyed out even after saving the target configuration.
I didn't test jtag on the evm before I changed the jumpers. So I don't know if something is wrong there. Is there a specific jumper that would disable the onboard jtag?
I do have an XDS200 emulator that I connected to the jtag header on the board. The test connection button worked, but when I went to use it, CCS complained about not having a licence.
Anyone have a solution?
-Stef