Tool/software: Code Composer Studio
Dear All,
I am using circuit board of TMS320VC5505 eZDSP USB STICK (Revision B) and information on it can be found at support.spectrumdigital.com/.../.
I downloaded CCSv4 from http://support.spectrumdigital.com/boards/usbstk5505/revb/ Then created new target configuration with "Connection" as "Texas Instruments XDS100 USB Emulator" and "Board or Device" as "USBSTK5505".
I can successfully connect ccs to TMS320VC5505 eZDSP USB STICK for debug purposes.
However, when I use CCSv6.1.3 and create new target configuration with "Connection" as "Texas Instruments XDS100v1 USB Debug Probe" and "Board or Device" as "USBSTK5505", I cannot connect to target. I get the error like
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 6.0.222.0)
I am not sure about the cause. I can connect to target using CCSv4 with "Connection" as "Texas Instruments XDS100 USB Emulator" but cannot using CCSv6.1.3 with "Connection" as "Texas Instruments XDS100v1 USB Debug Probe". Changing to "Texas Instruments XDS100v2 USB Debug Probe" or "Texas Instruments XDS100v3 USB Debug Probe" does not change the situation.
Would be great if anyone can help.
Thanks.