Tool/software: Code Composer Studio
I am using Version: 7.0.0.00043 and not able to view any "static" variable. Only able to view local variable.
Is there a way to examine Static ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For file statics, you can use a syntax in the expressions view like: '<file name>'::<static var name> (e.g. 'peripheral.c'::testvar2)Dilbert K said:Is there a way to examine Static ?
[Found on this thread https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/70217/255694#255694]
I tested CCS 7.3.0.00019 with a Cortex-A8 program built with the GNU v6.3.1 compiler.Dilbert K said:However, after enter, it always shows "identifier not found"
A source file named sdram_test_main.c had two static variables, one at file scope and another with function scope:
static uint32_t file_scope_var = 1; static void inc_static_var (void) { static uint32_t function_scope_var; function_scope_var = file_scope_var; file_scope_var++; }
In the expressions entered the variables twice:
a) Just using the variable name.
b) Qualifying the expression as:
'<source_filename>'::<variable_name>
When the debug context was in a function in the source file with the static variables, both types of expression displayed the value of the variables:
When the debug context was in a function in a different source file the expressions with just the variable name showed "identifier not found", but the expressions qualified with the file names did display the values:
Do you still get "identified not found" even when qualifying the expression with the name of the source file?
I tried below format
int8_t testing=88;
'main.c'::testing
and it only work without "static" being defined in variable.
Once static is defined, then it shows "identifier not found"
I wonder some setting in the CCS tools in build options, I need to enable