Part Number: MSP432P401R
Tool/software: Code Composer Studio
When Importing example using Resource Explorer "Error importing project. Device-id "Cortex M.MSP432P401R" is not recognized!"
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
When Importing example using Resource Explorer "Error importing project. Device-id "Cortex M.MSP432P401R" is not recognized!"
Tom,
This error is commonly seen when support for the device is not installed, so the first question would be whether you selected the MSP432 family of devices when initially installing CCS. If not, you can re-run the CCS installer and add the MSP432 device support.
Please see these two related threads:
https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/615892/2269554#2269554
https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/594781/2186361#2186361
The error message occurs when I try to "Import to IDE" i.e. left click on the CCS icon near top right corner of screen.
The Resource Explore is covered with the transparent GRAY overlay and the pop up error message. This happens for all of the different examples including the Register Level Examples. It also occurs for the "TI-RTOS for MSP43x - v:2.20.00.06 " sub-folder example projects.
I was able to create a new 432 project then cut paste the code from an example to get a working project that b links the LED on the MSP-EXP432L401R board.
I have also build a couple of 432 projects from scratch that 'blink the LED' etc.
BTW: CCS is Version 6.2.0.00050
Tom,
I'm a bit stumped as to why the import would fail with this error if you are able to create a new project for the same device. It looks like you are using MSP432Ware v3.50.00.02, is that correct? I just tried this out with CCS 6.2.0.00050 and MSP432Ware v3.50.00.02 and am able to import projects without any issues.
I wonder if there's something missing in your CCS installation. I know this isn't ideal but could you try reinstalling CCS 6.2?
Or better yet, if you are not locked into version 6.2, I would suggest upgrading to the latest CCSv7 and Simplelink MSP432 SDK which is the newer software package that supersedes MSP432Ware, so you can start your development with the most up-to-date versions of software and tools.