Tool/software: Code Composer Studio
Hello
I#m using CCSv7.3, now I’d like to install some add-ins, that I haven’t been able to yet.
The follow thinks happen with that version:
-
when I Open the App-Centre the CrashReportJob runs for ever
-
I can’t see any logo of the add ins
-
There is a kind of circle running for C2000 Compiler an so on (see picture CCS.jpg)
-
When I select the CVS add in and press Install Software the Operation starts but it freezes, I only can kill CCS than by the task manager (see picture CCS1.jpg)
I modified the Network connections (see picture CCS2.jpg) what is the proxy port that has to be used?
When I have a look at the available Software sites, this comes up (see picture CCS3.jpg)
When I try to open the http://software-dl.ti.com/ccs/esd/CCSv7/Updates directly by using a browser, the browser can’t find the page, all the other can be found – is that ok?
When I press Reload the operation starts as well, but it fails (see picture CCS4.jpg)
Thomas