Tool/software: Code Composer Studio
I got the following problem with updating CCS :
At the end I got this error message:
Can someone please tell me how to solve this.
Thanks,
EVS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We found there was problem where the 3rd party content delivery provider's data was out of sync with our local data. This issue has been corrected.
Could you retry this operation? The error message reported above looked like it might have been unrelated so we may still have something to investigate.
I suspected the sync issue was not going to resolve this.
Would you be able to exit CCS, then download and run the attached "installer". While it looks like an installer, all it does is patch some of the existing installation scripts that get run when you try to install an update. We are suspecting that a sequence of dependencies in your installs causes this problem. The patch relaxes those dependencies.
The installer asks for the install location of CCS and defaults to c:\ti. If you have installed in a different folder, you can point it to that folder.
After running the patch, please retry the update and let us know how it goes.
Re-Opening Code Composer after forced exit of updater window and requesting updates once more results in first: "No updates found" and at the same time an error message "No repository found at software-dl.ti.com/.../."
I got the flowing error from windows:
The program can not be started because COMCTL32.DLL is missing on your computer. You may be able to resolve this problem by reinstalling the program. (only in an other languages)
I got COMCTL32.dll 20 times on my PC.
Maybe compress the file. Because of firewalls.
On My Side, I installed your provide patch then the two update Compiler C2800 are ok now.
When I click on "Check For update" the two error message you said bellow was appeared.
So i restart CCS and now it indicate (No Updates were found in available software sites".
This Is Ok,
But I was tried this week to installe the CCS 7.3.0, with the same problem reported above.
Now in Help/About Code Composer Studio, the version field is blank!
I try to re installe CCS v7.3.0:
After it proposed to me to generat a report to Texas, It indicate:
"Submit completed, Use the reference number below to follow up on this issues using the online CCS support Forums. Reference #: 68753"..
I not find in the forum the section with the following of this submit..
Then after that, In Ccs, it ask me again to update ARM Compiler and C2800 Compiler, I click Ok, it install and after that ask me to restart CCS. Then the installation of Ccs v7.3.0 start again... And will crash like last time etc...
Referring only to A GIR's reply:
We had a look through the submitted logs. Prior to the initial problem, the installation was updated from 7.1 to 7.2, and had various other updates applied. These all went fine. The initial problem occurred Nov 6. There was an additional installation attempt to resolve the problem on Nov 14. The Nov 14 install attempt appears to have put the installation in an unrecoverable state where there were pieces of both the new install and the original install.
Rather than try to untangle the issues with the current installation folder, my recommendation would be start from a clean v7.3 installation. It would be best to rename or delete the prior installation folder before to starting (IE, rename C:\ti\ccsv7 to something else).
We are very sorry for the trouble and have taken steps to ensure the dependency issue you ran into on Nov 6 is addressed for CCS v7.4.
The CCS installer also includes and runs the Visual Studio 2015 redistributable installer from Microsoft. For some reason this redistributable installer is failing. This can be run by itself to better see what it is having trouble with.
You can get the same executable from Microsoft, or I've also made it available here. Please run this installer. If it offers to repair your installation, please allow it to do so. After this has successfully installed, what does the update do?