Tool/software: Code Composer Studio
Hello
I just install CCS v7.3.0 (By remove previous CCS installation v7.2.0)
But If I remember well, the problem exist also with v7.2.0..
CCS is always in a "C/C++ indexer : (xx%)":
I make this screenshot, and now, when I writing these lines, the progress is : Indexing: 2 250/2486, 18229 headers: (51%)
So this task never finish: Even when I'm compile of make debug.
I don't know what mean this task, but for me, my computer CPU load increase with this.
Currently, while CCS do nothing else (No debug, no compile...) , the CCS processus take on my computer more than 65% Cpu load!... This is too much!
Then When I use the debug, with other tool (CAN Analyser tool...) the CPU load is too much and the reaction time is very long!...
I don't think is my computer which is too old, because some month ago (< 1 month) I haven't this problem and CCS do not take these CPU Load (Core i5 vPro)
Can I resolve this?...
Thank