Tool/software: Code Composer Studio
Hello all iam having a bit of a problem trying to find a easier way including libraries.So far my steps are finding a header file in tirtos documentation for example ti/drivers/spi/SPICC26XXDMA.h then putting a
#include <ti/drivers/spi/SPICC26XXDMA.h> then i compile the code and if there is a error where it cant find the source file SPICC26XXDMA.h i find the correct folder were the header file is and add it in the Include Options under the C/C++ Build.Is there a way i can add all the libraries in my project without having to go one by one,or any other way to do it is welcomed.Thanks