Tool/software: Code Composer Studio
I am creating a RTSC Module and I wanted to design a interface whose parameter use the type uintptr_t.
The XDCtools even recognize the standard size_t type, but cannot read the types like uintptr_t, int32_t, etc.., which are also C standard types. Is there any workaround for this?
Maybe in future release, XDCtools could add support for all at least C99 standard types.
BTW: Even I have already done a lot of coding work related to XDC environment, I still feel that those XDC re-typedefed basic types are unnecessary. For example, 'void' is typedefed to 'Void'. Another example, C standard has already defined width-specific types in stdint.h, but xdc has its own UInt32, xdc_Int32, etc..I guess maybe to let the compiler do this part of thing is a good choice.
Maybe I didn't look at it from a overall view.