Tool/software: Code Composer Studio
Hello,
I currently have two separate CCS projects - one for the bootloader, and another for the firmware. Currently when I want to test/debug the the firmware, I first have to launch a debug session for the bootloader so it is flashed onto the microcontroller, then load the firmware out file (ensuring the debug configuration is set to only erase necessary flash sectors). I then have to add the bootloader symbols to the debug session again as they are dropped when loading in the firmware.
All of this is a bit of a hassle. Is it possible to automate the above steps so when I launch a debug session for the firmware, it automatically loads the bootloader too?
Many thanks