Other Parts Discussed in Thread: MSP430FR2422
Tool/software: Code Composer Studio
I am using CCS Version: 8.0.0.00016. In my code I have:
#pragma DATA_SECTION( EngSet, ".infoB" )
int EngSet = 250; // engine temperature set point
This places the variable in FLASH in the infoB section as can be seen in the Code.map file:
00001000 EngSet
The Code.txt file starts at @e000 and does not have any data located at @1000. I would like to have the EngSet variable initialized to 250 when I program the part. I will be changing the value of EngSet in the program (can't be declared const) but I need it initialized. I have tried several modification to lnk_msp430f123.cmd but they have not worked.