This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 and Windows 7 64-bit not working with Blackhawk USB 560bp emulator

I have CCS 4.1.3.00038 installed on a PC running 64-bit Windows 7.  Every time I try to start the debugger I get a dialog box that says "Error initializing emulator".  The Blackhawk emulator appears to be enumerating properly and shows up in Device Manager.  The output of the BHDetect utility is included below.  The same setup works fine on a Windows XP 32-bit machine.  I cannot find anything on the e2e site that says CCS4 should not work with windows 7 64 bit.  Is there something else I can look at to debug this problem?

Thank you,

--Bill

 

07:23:03: BHDetect - Version 1.0.0.9
07:23:03: 
07:23:03: Scan started on Monday, October 11, 2010 at 07:23:03 AM.
07:23:03: 
07:23:03: MEYEMAC
07:23:03: wsm
07:23:03: 
07:23:03: Starting Quick Scan for CCStudio Installations...
07:23:03: 
07:23:03: %%ERROR: bhDetect_GetIniFile() opening ComponentManager registry key.
07:23:03: bhDetect_ListCCSInstallations:  Error locating CCStudio Component Manager INI file.
07:23:03: bhDetect_ListCCSInstallations:  No valid CCS installations found.
07:23:04: 
07:23:04: Starting scan for installed Blackhawk Driver Files...
07:23:04: 
07:23:04:                       blackhwk.cpl, v01.01.00.00,     266280 bytes, Mon Mar 23 11:26:08 2009
07:23:04: 
07:23:04:       Processing SYS Files...
07:23:04:                       bh510usb.sys, v01.14.00.00,     310568 bytes, Mon Mar 23 11:26:06 2009
07:23:04:                       bh560eth.sys, v01.00.00.09,      97704 bytes, Thu Jan 15 14:10:36 2009
07:23:04:                       bh560usb.sys, v01.09.00.00,     318248 bytes, Mon Mar 23 11:26:08 2009
07:23:04:                          bhpci.sys, v01.05.00.00,     481448 bytes, Mon Mar 23 11:26:08 2009
07:23:04: 
07:23:04: Starting scan for Blackhawk Emulators...
07:23:04: 
07:23:04:    1.) Blackhawk USB560-BP JTAG Emulator (S/N:LF4521)
07:23:04: 
07:23:04: Completed scan for Blackhawk Emulators.
07:23:05: 
07:23:05: Scan Completed Successfully on Monday, October 11, 2010 at 07:23:05 AM.
07:23:05: 
07:23:05: ******************************************************************************
07:23:05: BHDetect - Version 1.0.0.9    Errors: 1,  Warnings: 0
07:23:05: ******************************************************************************
07:23:05: BHDetect has completed a scan of your system.  The output generated in the
07:23:05: dialog box window is designed to help debug installation and setup problems.
07:23:05: Any messages that begin with "%ERROR" should be addressed and you can
07:23:05: contact Blackhawk support via email: support@blackhawk-dsp.com and include
07:23:05: the output from this utility for faster response.
07:23:05: 
07:23:05: Thank you,   The Blackhawk Support Team.
07:23:05: ***************************************************************************EOF.

 

 

14 Replies

  • Guru 143155 points

    Bill,

    CCS 4.1.3 should work with Windows 7, but it is recommended to install CCS outside the "Program Files" or "Program Files (x86)" directory as mentioned here:
    http://processors.wiki.ti.com/index.php/Running_CCStudio_v3.3_on_Windows_Vista#CCSv4

    What device are you connecting to? Does connection to the same device with the same emulator work with from the Windows XP machine with the same version of CCS (4.1.3)?

     

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    I have installed CCS4 in  C:/TI.  I'm trying to connect to a TMS320C6747.  I am using the same CCS version, emulator, and board with Windows XP.  The only curious thing  in my 64-bit setup is that the Blackhawk detect utility says it can't find a valid install of CCS (see previous post), even though it's definitely installed.

    Thank you,

    --Bill

     

  • Guru 124460 points

    In reply to Bill McKinney:

    Bill,

    The utility from BlackHawk is trying to detect a CCSv3.3 installation, thus the error (it found one in my PC as I have both 3.3 and 4 installed). Because of this I am not sure if the information provided is reliable with the updated device drivers for CCSv4 (in my Win7/64 this utility does not give me any information about the driver files!).

    Even still, to help get additional details about this issue could you please use the tool <dbgjtag.exe> from your CCSv4 installation and publish the results? Its usage is described in the link below:

    http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems#CCS_v4

    BTW, I use a BH560m (not bp) in my Win7/64 and OMAPL137 without trouble.

    Hope this helps,

    Rafael


    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

    Search the wiki or go to useful pages for SDOWP, Compilers, CCSv3, CCSv4, CCSv5, CCSv6, CCSv7
  • In reply to desouza:

    Thanks for the very prompt response.  I appreciate it.  One thing I neglected to mention is that the board i'm using has the DSP in a jtag chain with a couple of other devices.  The DSP is not the first device in the chain.  Have you had any experience on Windows 7 with boards with the processor in a jtag chain?

    I'll get you the results as soon as I can.

    Thanks again,

    --b

     

  • Guru 124460 points

    In reply to Bill McKinney:

    Bill,

    No, I haven't used any other devices in daisy-chain with this specific DSP. However the CCSv4 target configuration file (.ccxml) will have to reflect that.

    In your case you will have to create the JTAG configuration by adding each daisy-chained device in order - they would be either a DSP (for the C6747) or a bypass device with "x" number of bits (for each of the other ones). Please check the page below that contains additional details on how to create a custom configuration:

    http://processors.wiki.ti.com/index.php/Target_Configuration_-_Custom_Configurations

    Hope this helps,

    Rafael


    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

    Search the wiki or go to useful pages for SDOWP, Compilers, CCSv3, CCSv4, CCSv5, CCSv6, CCSv7
  • In reply to desouza:

    The target configuration file I have works fine with 32-bit Windows XP.  I'm using the same config with Windows 7 64-bit, but can never get past the emulator initialization.

    Thanks again,

    --b

     

  • In reply to desouza:

    I ran dbgjtag as follows:

    /TI/ccsv4/common/uscif/dbgjtag.exe -f 'C:\TI\ccsv4\DebugServer\bin\win32\BrdDat\ccBoard0.dat' -rv -S pathlength

    It reported the following:

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver.

    The value is '-131' (0xffffff7d).
    The title is 'SC_ERR_SYS_MEM_ALLOC'.

    The explanation is:
    The operating system has reported a memory error when allocating memory.

     

    This is pretty odd.  There are no errors that I can find in any of the windows event logs.  I've got 8GB of memory in this machine.  Any ideas?

    Thanks again,

    --b

     

     

  • In reply to Bill McKinney:

    Should I just try reinstalling ccsv4?

  • Guru 143155 points

    In reply to Bill McKinney:

    Bill,

    Just some ideas on few other things to check:

    - Can you open the Blackhawk control panel (should be an icon on your desktop) and see if it detects your emulator correctly?

    - Run the reset and probe diagnostic utilities that Blackhawk provides.  There should be a BHreset_USB560bp.bat file and BHprobe_USB560bp.bat file in the directory <installdir>\emulation\Blackhawk\Utility\BHProbe.2

    - Try updating your drivers if they are not already on the latest version. You can check for Blackhawk driver updates from within CCS Help->Software updates->Find and Install.

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • Guru 124460 points

    In reply to AartiG:

    Bill,

    Sorry for the delay; we have found some issues with the emulators being used in Win7/64bits environments; can I send you a patch in a private message?

    Regards,

    Rafael 


    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

    Search the wiki or go to useful pages for SDOWP, Compilers, CCSv3, CCSv4, CCSv5, CCSv6, CCSv7

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.