I have CCS 4.1.3.00038 installed on a PC running 64-bit Windows 7. Every time I try to start the debugger I get a dialog box that says "Error initializing emulator". The Blackhawk emulator appears to be enumerating properly and shows up in Device Manager. The output of the BHDetect utility is included below. The same setup works fine on a Windows XP 32-bit machine. I cannot find anything on the e2e site that says CCS4 should not work with windows 7 64 bit. Is there something else I can look at to debug this problem?
Thank you,
--Bill
07:23:03: BHDetect - Version 1.0.0.9
07:23:03:
07:23:03: Scan started on Monday, October 11, 2010 at 07:23:03 AM.
07:23:03:
07:23:03: MEYEMAC
07:23:03: wsm
07:23:03:
07:23:03: Starting Quick Scan for CCStudio Installations...
07:23:03:
07:23:03: %%ERROR: bhDetect_GetIniFile() opening ComponentManager registry key.
07:23:03: bhDetect_ListCCSInstallations: Error locating CCStudio Component Manager INI file.
07:23:03: bhDetect_ListCCSInstallations: No valid CCS installations found.
07:23:04:
07:23:04: Starting scan for installed Blackhawk Driver Files...
07:23:04:
07:23:04: blackhwk.cpl, v01.01.00.00, 266280 bytes, Mon Mar 23 11:26:08 2009
07:23:04:
07:23:04: Processing SYS Files...
07:23:04: bh510usb.sys, v01.14.00.00, 310568 bytes, Mon Mar 23 11:26:06 2009
07:23:04: bh560eth.sys, v01.00.00.09, 97704 bytes, Thu Jan 15 14:10:36 2009
07:23:04: bh560usb.sys, v01.09.00.00, 318248 bytes, Mon Mar 23 11:26:08 2009
07:23:04: bhpci.sys, v01.05.00.00, 481448 bytes, Mon Mar 23 11:26:08 2009
07:23:04:
07:23:04: Starting scan for Blackhawk Emulators...
07:23:04:
07:23:04: 1.) Blackhawk USB560-BP JTAG Emulator (S/N:LF4521)
07:23:04:
07:23:04: Completed scan for Blackhawk Emulators.
07:23:05:
07:23:05: Scan Completed Successfully on Monday, October 11, 2010 at 07:23:05 AM.
07:23:05:
07:23:05: ******************************************************************************
07:23:05: BHDetect - Version 1.0.0.9 Errors: 1, Warnings: 0
07:23:05: ******************************************************************************
07:23:05: BHDetect has completed a scan of your system. The output generated in the
07:23:05: dialog box window is designed to help debug installation and setup problems.
07:23:05: Any messages that begin with "%ERROR" should be addressed and you can
07:23:05: contact Blackhawk support via email: support@blackhawk-dsp.com and include
07:23:05: the output from this utility for faster response.
07:23:05:
07:23:05: Thank you, The Blackhawk Support Team.
07:23:05: ***************************************************************************EOF.