Part Number: EZ430-F2013
Tool/software: Code Composer Studio
Hi,
I recently bought an EZ430-F2013 USB Stick and I'm trying to set up a new project but I don't understand how to setup the device connection.
I'm using Windows 7 Ultimate SP1 x64, the driver in use by the EZ430-F2013 is "MSP-FET430UIF - VCP" with a COM3 port associated.
The target device is "MSP430F2013" and inside the connection menu I have multiple choice:
- TI MSP430 USB1
- TI MSP430 USB2
- TI MSP430 USB3
- UARTConnection
With any of the firsts 3 the "identify" functionality return the following error:
Error initializing emulator:
No USB FET was found
By using the UARTConnection I need change the default config port from COM65 to COM3 but now I see another error:
Can't Initialize Target CPU: Failed to open COM3 at 9600 baud: open: cannot find the specified file
I miss to configure something? The guidelines are for CCS v7.
In that way I cannot debug the "Blink" example ...
Thanks,
Gabriele
Thanks,
Gabriele