Part Number: CCSTUDIO-KEYSTONE
Tool/software: Code Composer Studio
Hi,
We have a customer using CCS to create target connection with two Keystone K2E EVMs. Their setup is:
Ubuntu 16.04 64-bit OS
CCS7.4.0 linux version
TMDXEVM66AK2E
XDS200 on board emulator
They followed the link below:
http://software-dl.ti.com/ccs/esd/documents/sdto_ccs_multi-probe-debug.html
http://processors.wiki.ti.com/index.php/Target_Configuration_-_Custom_Configurations
So they defined the port number as "0" and "1" respectively for the two K2E EVMs using XDS 200 emulator. It never worked for them. For any individual EVM, they can connect. So this is not a HW issue.
I asked customer to do the same steps with Windows 10 machine, CCS version is 7.4.0. It always worked. We also tried locally with Windows 7 + CCS 6.1.3, it always worked.
Can you help to resolve the issue on Ubuntu machine as this is their main work enviornment?
Regards, Eric