Tool/software: Code Composer Studio
Hello community,
I made a program with Matlab/Simulink (2016b) and I load it on CCSv6.2. I've used the watch window to visualize my variables.
These are my questions:
- which variable should I pick from the .c file to visualize the ePWM generated?
- How can I visualize in the same graph (two or three) variables?
- When I try to visualize a sine wave, the graph obtained is as shown in the figure. Is there a particular configuration that I have to put forward?
Regards