Tool/software: Code Composer Studio
Hello,
I'm using a Beagleboard x-15 and CCS 8.1. Compiler version GNU v6.3.1 (Linaro). I have imported the MCASP DeviceLoopbackExample from "\ti\pdk_am57xx_1_0_10\packages\MyExampleProjects\MCASP_DeviceLoopback_evmAM572x_armExampleProject" to my workspace and was able to build it. I created a target configuration which looks as follows:
When I launch the targetConfiguration my "NewTargetConfiguration.ccxml"-console prints following error:
Cortex_M4_IPU1_C0: GEL Output: --->>> AM572x Cortex M4 Startup Sequence In Progress... <<<--- Cortex_M4_IPU1_C0: GEL Output: --->>> AM572x Cortex M4 Startup Sequence DONE! <<<--- Cortex_M4_IPU1_C1: GEL Output: --->>> AM572x Cortex M4 Startup Sequence In Progress... <<<--- Cortex_M4_IPU1_C1: GEL Output: --->>> AM572x Cortex M4 Startup Sequence DONE! <<<--- Cortex_M4_IPU2_C0: GEL Output: --->>> AM572x Cortex M4 Startup Sequence In Progress... <<<--- Cortex_M4_IPU2_C0: GEL Output: --->>> AM572x Cortex M4 Startup Sequence DONE! <<<--- Cortex_M4_IPU2_C1: GEL Output: --->>> AM572x Cortex M4 Startup Sequence In Progress... <<<--- Cortex_M4_IPU2_C1: GEL Output: --->>> AM572x Cortex M4 Startup Sequence DONE! <<<--- C66xx_DSP1: GEL Output: --->>> AM572x C66x DSP Startup Sequence In Progress... <<<--- C66xx_DSP1: GEL Output: --->>> AM572x C66x DSP Startup Sequence DONE! <<<--- C66xx_DSP2: GEL Output: --->>> AM572x C66x DSP Startup Sequence In Progress... <<<--- C66xx_DSP2: GEL Output: --->>> AM572x C66x DSP Startup Sequence DONE! <<<--- CortexA15_0: GEL Output: --->>> AM572x Cortex A15 Startup Sequence In Progress... <<<--- CortexA15_0: GEL Output: --->>> AM572x Cortex A15 Startup Sequence DONE! <<<--- CortexA15_1: GEL Output: --->>> AM572x Cortex A15 Startup Sequence In Progress... <<<--- CortexA15_1: GEL Output: --->>> AM572x Cortex A15 Startup Sequence DONE! <<<--- IcePick_D: GEL Output: Ipu RTOS is released from Wait-In-Reset. IcePick_D: GEL Output: Ipu SIMCOP is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD C66 is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD ICONT1 is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD ICONT2 is released from Wait-In-Reset. CS_DAP_DebugSS: GEL Output: --->>> CONFIGURE DEBUG DPLL settings to 1.9 GHZs <<<--- CS_DAP_DebugSS: GEL Output: > Setup DebugSS 1.9GHz in progress... CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS PLL Clocking 1.9GHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS ATB Clocking 380MHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz CS_DAP_DebugSS: GEL Output: --->>> TURNING ON L3_INSTR and L3_3 clocks required for debug instrumention <<<<<<---- CS_DAP_DebugSS: GEL Output: ---<<< L3 instrumentation clocks are enabled >>>> --- CS_DAP_DebugSS: GEL Output: --->>> Mapping TIMER supsend sources to default cores <<<<<<---- CS_DAP_PC: GEL Output: Cortex-A15 1 is not in WIR mode so nothing to do. CortexA15_0: GEL Output: --->>> AM572x GP EVM <<<--- CortexA15_0: GEL Output: --->>> AM572x Target Connect Sequence Begins ... <<<--- CortexA15_0: GEL: Error while executing OnTargetConnect(): Target failed to read 0x4A0025F4 at (*((unsigned int *) 0x4A0025F4)&0xFFF) [AM572x_startup_common.gel:69] at AM57xx_EVM_Initialization(0) [gpevm_am572x.gel:54] at OnTargetConnect()
I am still able to connect to the CortexA15_0 by right click and connect to target. I clicked Run > Load > LoadProgram and select my .out file. Now I get the following message in my "NewTargetConfiguration.ccxml"-console :
CortexA15_0: GEL Output: --->>> Reset occurs <<<--- CortexA15_0: GEL Output: --->>> AM572x PG2.0 GP device <<<---
In the debug view I can see:
Also an new window shows up:
When I disconnect to CortexA_0 + reconnect and klick "restart" I get following messages:
IcePick_D: GEL Output: Ipu RTOS is released from Wait-In-Reset. IcePick_D: GEL Output: Ipu SIMCOP is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD C66 is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD ICONT1 is released from Wait-In-Reset. IcePick_D: GEL Output: IVAHD ICONT2 is released from Wait-In-Reset. CS_DAP_DebugSS: GEL Output: --->>> CONFIGURE DEBUG DPLL settings to 1.9 GHZs <<<--- CS_DAP_DebugSS: GEL Output: > Setup DebugSS 1.9GHz in progress... CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS PLL Clocking 1.9GHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS ATB Clocking 380MHz CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz CS_DAP_DebugSS: GEL Output: --->>> TURNING ON L3_INSTR and L3_3 clocks required for debug instrumention <<<<<<---- CS_DAP_DebugSS: GEL Output: ---<<< L3 instrumentation clocks are enabled >>>> --- CS_DAP_DebugSS: GEL Output: --->>> Mapping TIMER supsend sources to default cores <<<<<<---- CS_DAP_PC: GEL Output: Cortex-A15 1 is not in WIR mode so nothing to do. CortexA15_0: GEL Output: --->>> AM572x GP EVM <<<--- CortexA15_0: GEL Output: --->>> AM572x Target Connect Sequence Begins ... <<<--- CortexA15_0: GEL Output: --->>> I2C Init <<<--- CortexA15_0: GEL Output: --->>> AM572x Begin MMC2 Pad Configuration <<<--- CortexA15_0: GEL Output: --->>> AM572x End MMC2 Pad Configuration <<<--- CortexA15_0: GEL Output: --->>> AM572x PG2.0 GP device <<<--- CortexA15_0: GEL Output: --->>> PRCM Clock Configuration for OPPNOM in progress... <<<--- CortexA15_0: GEL Output: Cortex A15 DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: Cortex A15 DPLL is already locked, now unlocking... CortexA15_0: GEL Output: Cortex A15 DPLL OPP 0 is DONE! CortexA15_0: GEL Output: IVA DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: IVA DPLL OPP 0 is DONE! CortexA15_0: GEL Output: PER DPLL OPP 0 clock config in progress... CortexA15_0: GEL Output: PER DPLL already locked, now unlocking CortexA15_0: GEL Output: PER DPLL OPP 0 is DONE! CortexA15_0: GEL Output: CORE DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: CORE DPLL OPP already locked, now unlocking.... CortexA15_0: GEL Output: CORE DPLL OPP 0 is DONE! CortexA15_0: GEL Output: ABE DPLL OPP 0 clock config in progress... CortexA15_0: GEL Output: ABE DPLL OPP 0 is DONE! CortexA15_0: GEL Output: GMAC DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: GMAC DPLL already locked, now unlocking.... CortexA15_0: GEL Output: GMAC DPLL OPP 0 is DONE! CortexA15_0: GEL Output: GPU DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: GPU DPLL OPP 0 is DONE! CortexA15_0: GEL Output: DSP DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: DSP DPLL OPP 0 is DONE! CortexA15_0: GEL Output: PCIE_REF DPLL OPP 0 clock config is in progress... CortexA15_0: GEL Output: PCIE_REF DPLL already locked, now unlocking.... CortexA15_0: GEL Output: PCIE_REF DPLL OPP 0 is DONE! CortexA15_0: GEL Output: --->>> PRCM Clock Configuration for OPP 0 is DONE! <<<--- CortexA15_0: GEL Output: --->>> PRCM Configuration for all modules in progress... <<<--- CortexA15_0: GEL Output: --->>> PRCM Configuration for all modules is DONE! <<<--- CortexA15_0: GEL Output: --->>> DDR3 Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DDR DPLL clock config for 532MHz is in progress... CortexA15_0: GEL Output: DDR DPLL already locked, now unlocking.... CortexA15_0: GEL Output: DDR DPLL clock config for 532MHz is in DONE! CortexA15_0: GEL Output: Launch full leveling CortexA15_0: GEL Output: Updating slave ratios in PHY_STATUSx registers CortexA15_0: GEL Output: as per HW leveling output CortexA15_0: GEL Output: HW leveling is now disabled. Using slave ratios from CortexA15_0: GEL Output: PHY_STATUSx registers CortexA15_0: GEL Output: Launch full leveling CortexA15_0: GEL Output: Updating slave ratios in PHY_STATUSx registers CortexA15_0: GEL Output: as per HW leveling output CortexA15_0: GEL Output: HW leveling is now disabled. Using slave ratios from CortexA15_0: GEL Output: PHY_STATUSx registers CortexA15_0: GEL Output: Two EMIFs in interleaved mode - (2GB total) CortexA15_0: GEL Output: --->>> DDR3 Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> Mapping TIMER suspend sources to default cores <<<<<<---- CortexA15_0: GEL Output: --->>> IPU1SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> IPU1SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> IPU2SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> IPU2SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> DSP1SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! CortexA15_0: GEL Output: --->>> DSP1SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> DSP2SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! CortexA15_0: GEL Output: --->>> DSP2SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> IVAHD Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: --->>> IVAHD Initialization is DONE! ... <<<--- CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in complete ... <<<--- CortexA15_0: GEL Output: --->>> AM572x Target Connect Sequence DONE !!!!! <<<--- CortexA15_0: GEL Output: --->>> Mapping TIMER suspend sources to default cores <<<<<<---- CortexA15_0: GEL Output: --->>> IPU1SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> IPU1SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> IPU2SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> IPU2SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> DSP1SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! CortexA15_0: GEL Output: --->>> DSP1SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> DSP2SS Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! CortexA15_0: GEL Output: --->>> DSP2SS Initialization is DONE! <<<--- CortexA15_0: GEL Output: --->>> IVAHD Initialization is in progress ... <<<--- CortexA15_0: GEL Output: DEBUG: Clock is active ... CortexA15_0: GEL Output: --->>> IVAHD Initialization is DONE! ... <<<--- CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in progress ... <<<--- CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in complete ... <<<---
And nothing happens..
I think I made a mistake in my configurations somewhere, but I can't figure out where. Does anyone knows who to solve this issue?
https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/658821?CCS-AM5728-GEL-error-while-executing-OnTargetConnect says "The GEL file is designed for the AM572x EVM" which I am using, so I assume this can't resolve my problem.
https://e2e.ti.com/support/arm/sitara_arm/f/791/p/558262/2046170#2046170 says that "we recommend you use CCS 6.1.3" which I tried, but ran into other issues. I checked every command that was given as a support and I have all the wished settings. The post ends with the same issue that I have.
Thanks in advance,
Frederic