Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
HI,
I think i encounter the same problem in this thread
my ccs was version 8.1.0
i try to import the empty rtos example in resource explorer ,
however, it comes to error as below:
**** Build of configuration Debug for project tirtos_builds_CC1310_LAUNCHXL_release_ccs ****
"E:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
making ../src/sysbios/rom_sysbios.aem3 ...
gmake[1]: Entering directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
asmem3 C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch.sv7M ...
gmake[1]: Leaving directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
gmake[1]: Entering directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
asmem3 C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm.sv7M ...
gmake[1]: Leaving directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
gmake[1]: Entering directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
asmem3 C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M ...
7 Assembly Errors, 1 Assembly Warning
>> Compilation failure
makefile:42: recipe for target 'm3_Hwi_asm.obj' failed
"C:\ti\simplelink_cc13x0_sdk_2_20_00_38\kernel\tirtos\packages\ti\sysbios\family\arm\m3\package/internal/Hwi.xdc.h", line 15: fatal error: cannot open source file "ti/sysbios/family/arm/m3/Hwi.h"
Compilation terminated.
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", WARNING! at line 37:
[E1000]
error while processing C code in .cdecls directive
.cdecls C,NOLIST,"package/internal/Hwi.xdc.h"
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 53:
[E0004]
Structure/Union tag symbol expected
ti_sysbios_family_arm_m3_Hwi_Module__state__V .tag ti_sysbios_family_arm_m3_Hwi_Module_State
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 99:
[E0004]
Absolute, well-defined integer value expected
.if ti_sysbios_Build_useIndirectReferences
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", REMARK at line 99:
[R0001]
After symbol substitution the line became:
.if FALSE
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 160:
[E0004]
Absolute, well-defined integer value expected
.if ti_sysbios_Build_useIndirectReferences
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", REMARK at line 160:
[R0001]
After symbol substitution the line became:
.if FALSE
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 263:
[E0004]
Absolute, well-defined integer value expected
.if ti_sysbios_Build_useIndirectReferences
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", REMARK at line 263:
[R0001]
After symbol substitution the line became:
.if FALSE
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 267:
[E0009]
Missing struct/union member or tag
swiTaskKeyAddr: .word ti_sysbios_family_arm_m3_Hwi_Module__state__V.swiTaskKeys
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at line 289:
[E0004]
Absolute, well-defined integer value expected
.if ti_sysbios_BIOS_smpEnabled__D
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", REMARK at line 289:
[R0001]
After symbol substitution the line became:
.if FALSE
"C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M", ERROR! at EOF:
[E0300]
The following symbols are undefined:
FALSE
swiTaskKeys
ti_sysbios_family_arm_m3_Hwi_Module_State
ti_sysbios_family_arm_m3_Hwi_Module__state__V
Errors in Source - Assembler Aborted
gmake[1]: *** [m3_Hwi_asm.obj] Error 1
gmake[1]: Leaving directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
gmake[1]: Entering directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
asmem3 C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/family/arm/m3/TaskSupport_asm.sv7M ...
gmake[1]: Leaving directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
gmake[1]: Entering directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
clem3 C:/ti/simplelink_cc13x0_sdk_2_20_00_38/kernel/tirtos/packages/ti/sysbios/BIOS.c ...
makefile:59: recipe for target 'rom_sysbios.obj' failed
gmake[1]: *** [rom_sysbios.obj] Error -1073741502
gmake[1]: Target 'all' not remade because of errors.
gmake[1]: Leaving directory 'E:/Projects/water_meter/ti_sw/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios'
../src/makefile.libs:56: recipe for target '../src/sysbios/rom_sysbios.aem3' failed
gmake: *** [../src/sysbios/rom_sysbios.aem3] Error 2
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Can someone help?
thanks
Jeff