Hi TI,
Is this a bug of CGTv4.9.1 ?
BR, Yulin.
---- detail ----------------------------------------------------------
typedef enum{ PSL_DISABLED = 0, // Don't do any power saving PSL_BACKLIGHT = 1, // Can turn off LCD backlight PSL_DISPLAY = 2, // Can turn off screen power & LCD clocks PSL_SYSPOWER = 3 // Can turn off system power}TPS;
The argument "level" must be an unsigned type. And, by definition, an unsigned variable is always greater than or equal to 0. So, the compiler is trying to tell you that the test "level >= PSL_DISABLED" is always true. Next time, add --verbose_diagnostics to your build. That will help you see the problem. For more discussion on diagnostics and how to handle them, see the diagnostics section of this presentation on the Wiki.
Thanks and regards,
-George
TI C/C++ Compiler Forum ModeratorPlease click Verify Answer on the best reply to your question.The Compiler Wiki answers most common questions.Track an issue with SDOWP. Enter your bug id in the "Find Record ID" box.
Hi Georgem,
Thanks for taking care of this.
I know it is due to the test "level >= PSL_DISABLED" is always true.
However, the function declaration "void psc_SetPowerSaveLevel(TPS level)" specifies 'level' to a TPS type instead of unsigned.
What's wrong then ?
BR,
Yulin.
YulinHowever, the function declaration "void psc_SetPowerSaveLevel(TPS level)" specifies 'level' to a TPS type instead of unsigned.
Ah. I overlooked that. I suppose you could say the error message text is bit misleading. Perhaps it should say something like the enum comparison is always true. But that's a small thing, really. The main point is that the comparison "level >= PSL_DISABLED" is always true. So it is still legitimate for the compiler to issue a diagnostic.
I was under the impression that enums usually of the type "int"? The diagnostic would imply enums are "unsigned int". That would mean you could not specify a negative values in the enumeration?
Both 'level' and 'PSL_DISABLED' is of type enum TPS and enum is int by default.
Why does compiler consider 'level' unsigned ?
I changed nothing about enum in the compiler options.
Thanks & regards,
In GCC mode, the underlying type is considered unsigned if none of the enumeration constants is negative.
I will not guess as to why this is so.