Hi all,
how can i genarate a coff file with CCS 5.1?
and why are C2000 DSP's not supportet for ELF/DWARF format, which would be even better for me right now?
Greetings
S.Fischer
If you are building for C2000, the default output generated in CCS5.1 will be COFF. We currently have ELF support for other platforms like C6000, ARM, MSP430, but not for C2000. ELF support for C2000 will be coming in the future but I'm not sure of the time frame.
If a post answers your question please mark it with the "Verify Answer" button
Search the wikis for common questions: CGT, BIOS, CCSv3, CCSv4Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box
So my .out File is allready coff format little confusing ?
Yes it should be COFF.
Is ELF support for C2000 now available. If not, when is it planned ?
Daufeld GhislainIs ELF support for C2000 now available.
No.
Daufeld GhislainIf not, when is it planned ?
None of the present plans include ELF. We may add ELF support eventually, but that has not been determined yet.
Thanks and regards,
-George
TI C/C++ Compiler Forum ModeratorPlease click Verify Answer on the best reply to your question.The Compiler Wiki answers most common questions.Track an issue with SDOWP. Enter your bug id in the "Find Record ID" box.