This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Linux/TDA3XEVM: INTERNAL ERROR

Part Number: TDA3XEVM

Tool/software: Linux

Hi there,

I am trying to build the application for TDA3x evm (building it for the first time) using "PROCESSOR_SDK_VISION_03_03_00_00_setuplinux" , after made changes in ../vision_sdk/build/Rules.make to set MAKEAPPNAME=apps and MAKECONFIG=tda3xx_evm_bios_all.(using ubuntu 14.04, os-type=64 bit)

In terminal ../vision_sdk/build$ make -s -j depend (compiled successfully)

and doing "make -s -j" i am experiencing an error with is mentioned below:

=========================================================================

INTERNAL ERROR: (native_path)/PROCESSOR_SDK_VISION_03_03_00_00/PROCESSOR_SDK_VISION_03_03_00_00_setuplinux/ti_components/cg_tools/linux/arp32_1.0.7/bin/acpia-arp32 experienced a segmentation fault while
                processing

This is a serious problem.  Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.


>> Compilation failure
=========================================================================

Why does this happen? How can I solve these  issue?

Thanks in advance

With Regards

Balaji

  • In reply to Rishabh Garg:

    Hi Rishabh,

    Here is the conf of my pc,
    =====================================
    balaji@FSETBLR1D036:~$ uname -a
    Linux FSETBLR1D036 4.2.0-42-generic #49~14.04.1-Ubuntu SMP Wed Jun 29 20:22:11 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux
    =====================================

    Regards
    Balaji T
  • In reply to balaji t:

    Hi Balaji,

    I tried the build on Ubuntu 14.04.5 and it worked fine for me.
    Can you please check if the build works for you on another machine or using a fresh installation on same machine.

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi Rishabh,

    I am using another PC with "Linux FSETBLR1LX046 4.4.0-57-generic #78~14.04.1-Ubuntu SMP Sat Dec 10 00:14:47 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux" configuration, in that i made build many time without any error.

    But my PC is with "Linux FSETBLR1D036 4.2.0-42-generic #49~14.04.1-Ubuntu SMP Wed Jun 29 20:22:11 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux", gives the error every time.

    Does kernel versions 4.4 and 4.2 makes any sense? can i do upgrade my kernel to  Linux 4.4.0-57 and try build again? 

    I want to find the reasons for this error, because i have another project using TDA2Echo board, In that also while building "make -s" i am getting the same error. so please look into this issue very seriously.

    regards

    balaji t

  • In reply to balaji t:

    Hi Balaji,

    we are not able to come up with any reason why it works on one machine and there is segmentation on another one, so I will move the thread to Compilers forum. Hopefully the experts there can give some help.

    Regards,
    Yordan
  • In reply to Yordan Kamenov:

    Hi Yordan,

    I would really like to appreciate this help from you,

    Regards
    Balaji T
  • In reply to balaji t:

    Hi there,

    Is there any update..?

    regards

    Balaji T

  • In reply to balaji t:

    I suspect you are experiencing compiler bug CODEGEN-2098.  In some circumstances, multiple compilations in parallel may use the same temporary file name, with unpredictable results.  See the Target Release part of the bug entry for the list of compiler versions which implement the fix.  Be sure all the compilers you use are of one of those versions, or later.

    Thanks and regards,

    -George


    TI C/C++ Compiler Forum Moderator
    Please click This Resolved My Issue on the best reply to your question
    The CCS Youtube Channel
     has short how-to videos
    The 
    Compiler Wiki answers most common questions
    Track an issue with SDOWP. Enter your bug id in the Search box.

  • In reply to George Mock:

    Hi George,

    Upgrading compilers may resolve my issue..??

    regards

    Balaji T

  • In reply to balaji t:

    Hi Balaji,

    Yes. Can you use the compilers mentioned under "Target Release" in the Incident report mentioned above.

    Regards,
    Rishabh
  • In reply to Rishabh Garg:

    Hi Balaji,

    Is this issue resolved?

    Regards,
    Rishabh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.