We have an issue while trying to compile .asm files on the C674X DSP,
We have a DSP out file, which depend on a certain lib (coded in assembly), the issues is:
When I have a .asm file which is compiled in the lib -> while linking the DSP out file, I’m getting undefined symbols (on the function in the .asm file)
When I move the .asm file to compile as part of the DSP out makefile, I’m getting the same result
When I move the .asm file to compile as part of the DSP out makefile AND change the function prefix (removing all ‘_’ at the beginning of the function name in the .asm file), all is OK
Is there any compiler option to allow taking '_' prefixed assembly functions and linking with C code?