Hello,
I am finding my way with CCS5.1 and got some trouble configuring new tools.
I have a legacy v3.3 project. I have imported it to CCS 5.1.1 using import legacy project wizard.
In my previous project I have custom linker file. At the beginning of memory image we define 3 custom sections for primary bootloader, secondary boot and program image descriptor. To do that we used command file with following commands:
custom.cmd:SECTIONS { .init_booting: {} > primary_boot .booting: {} > main_boot .info: {} > prg_info }
Source file for bootloader contains
#pragma CODE_SECTION (primary_loader, ".init_booting"); #pragma CODE_SECTION (boot_main, ".booting");
and info section contents is defined elsewhere. We used to mentioned above custom.cmd as linker input and it worked fine. Now with ccs 5.1 it does not work. I have specified that linked command file in Project\Properties\General\Linker command file. But assembled image is wrong. Here is excerpt from the map file:
MEMORY CONFIGURATION name origin length used unused attr fill ---------------------- -------- --------- -------- -------- ---- -------- primary_boot 00000000 00000100 00000000 00000100 RWIX main_boot 00000100 00000200 00000000 00000200 RWIX prg_info 00000300 00000010 00000010 00000000 RWIX IRAM 00000320 0007fce0 00076454 0000988c RWIX IHRAM 00080000 00080000 00080000 00000000 RWIX
So as one can see, primary_boot and main_boot sections are just empty. Moreover, there is unintended .vers section created and 0x0 and space from 0x0 to 0x320 is occupied by wrong code.
SECTION ALLOCATION MAP output attributes/ section page origin length input sections -------- ---- ---------- ---------- ---------------- .vers 0 00000000 00000038 COPY SECTION 00000000 00000038 myprj_cfg.obj (.vers) $BRID 0 00000000 000005a8 COPY SECTION 00000000 00000014 csl6416.lib : csl.obj ($BRID) 00000014 000000e4 : csl_edma.obj ($BRID) 000000f8 00000064 : csl_gpio.obj ($BRID) 0000015c 000002c0 : csl_tcp.obj ($BRID) 0000041c 00000064 : csl_timer.obj ($BRID) 00000480 000000b0 : csl_vcp.obj ($BRID) 00000530 00000078 : csl_irq.obj ($BRID) .info 0 00000300 00000010 00000300 00000010 info.obj (.info)
I am sure booting.c was compiled and I see booting.obj in the output directory. It just was not linked properly. Please advise, how to resolve.
I would start by comparing the build commands for CCS 3.3 and 5.1.1 specifically the link step. I suspect that in 5.1.1, it may be picking up another linker command file in addition (or in place of) your custom linker command file, or there are multiple files and somehow the link order is affecting the section placement. In CCS 3.3, the link command will be in the file Debug.lkf. In CCS 5.1.1 you can see it in the CCS build console. Try comparing these and see if you can spot a difference.
If you are unable to isolate the reason for the difference, please copy the full output of the CCSv5 build console on to a text file and attach it here. Also attach the link map file generated in CCSv5.
If a post answers your question please mark it with the "Verify Answer" button
Search the wikis for common questions: CGT, BIOS, CCSv3, CCSv4Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box
I had a trouble posting on the forum for a week, not it get fixed.
I made a big mistake and updated CGT for my CCS v3.3 and get it broken.So I removed source which was crashing compiler and got some output from 6.0.8 CGT. Linker command line in build option is-q -c -m"myproject.map" -o"myproject.out" -x -i"%BIOS_INSTALL_DIR%/packages/ti/rtdx/lib/C6000" -l"csl6416.lib"Excerpt from map file is attached as v6.0.08.map. As one can see, .init_booting, .booting and .info sections contain data in them and allocation is as expected. Also boot_main function, which is expected to be linked in main_boot section is found in symbols list with expected address 0x100.Now let's see v5.1 output. In attached out7.3.5.txt there is excerpt of output console.Command line follows prescribed patterncl6x--run_linker{--rom_model | --ram_model}filenames [options] [--output_file= name.out] --library=library [lnk.cmd]I see my custom link file is specified as last argument. However, there is -l"myprojectcfg.cmd" option specified before input object files. As I understand, it defines DSP/BIOS stuff linking. If we look inside generated map file (v7.3.5.map), only .prg_info section has correct data, others seems to be unused. Moreover, in the section allocation map we see, that at 0x0 there is unexpected there.vers 0 00000000 00000038 COPY SECTION.I know where it comes from. In the above mentioned -l"myprojectcfg.cmd" there is a command/* MODULE GBL */SECTIONS { .vers (COPY): {} /* version information */}So, my trouble is that cmd file of DSP/BIOS is get linked before my custom command file. In the same time, my command file is not processed properly. Function boot_main does not go to expected 0x100, it is not even mentioned in symbols list.
I noticed that this behaviour happen first time when I switched from 6.0.x CGT to 6.1.x. Could you guess, what I missed in my linker command file?
Thanks in advance.
rrlagicSo, my trouble is that cmd file of DSP/BIOS is get linked before my custom command file. In the same time, my command file is not processed properly. Function boot_main does not go to expected 0x100, it is not even mentioned in symbols list.
Did you compare the build command line from CCS 5.1 with the one from CCS 3.3? I see that you attached the output build console for CCS 5.1 but not the one from CCS 3.3. The key things to check are whether the same set of files (.obj + .lib) are being passed to the linker and the order of linker command files(if there is more than one).
Another test to perform might be use CGT 6.0.8 with CCSv5.1 and confirm if the map file is as expected. This could help determine if the issue is in the way the project was migrated to CCSv5 (which is what I suspect) or is in the CGT 7.3.x itself. The steps to use a different version of CGT with CCSv5 is documented here.
I have seen in a couple of cases where a CCS 3.3 project migrated to CCSv5 may require the link order of files to be re-specified in order to achieve the desired link result. In CCSv5, you can specify the order in which files are to be linked by going into Project Properties->CCS Build->Link Order tab. Depending on the complexity of the project and the way it was originally set up, the import tool in CCSv5 sometimes does not do a perfect job in the migration, thereby requiring some additional custom modifications to get an equivalent project.
Thank you for response. I attach .lkf file of my 3.3 project, there is a command line to linker.
As to 5.1, already I tried 6.0.x CGT. No surprise, with that version of CGT my project is linked correctly. But trouble is that with 6.0.x CGT the RTA does not work. With 7.3.5 I get RTA working, but boot code is missing due to linker issue.
In my 3.3 project I do specify linking order and put my custom linker command file before generated one. I do the same in 5.1, but it does not help. Again, if I try CGT of 6.1.x and above on 3.3, then linking is wrong. So I suspect there was some linker behaviour change between 6.0.x and 6.1.x, which I missed and noticed only on 7.3.5.
Can you suggest, where to look more?
Thanks
Can you attach the 2 linker command files (your custom one and the BIOS generated one) as well as the link map files generated with CGT 6.0.x and 7.3.x? That may give us more clues.
I attach two map files, linker command files and makefile found in debug folder of v5.1 project.
Thanks you for assistance.
According to the 6.0.29 map file, the object file booting.obj should have sections .init_booting and .booting. Can you check that those sections exist in the booting.obj file generated with 7.3.x? To do this, you can run ofd6x on the .obj file and check if the output file has these sections. Open a command prompt and run the following:ofd6x -g booting.obj > booting_ofd.txt
You may need to specify the paths to ofd6x (which is in the \bin folder within the compiler tools directory) and booting.obj. Then open the booting_ofd.txt and check if those sections are present.
If they are, the next thing to try is to add boot.cmd directly to the project instead of lte.cmd which in turn adds boot.cmd, and see if that makes a difference.
Ultimately, it might be easier for us to analyze further if we had the complete project along with all source/object files. Are you able to share the complete project so we can build it at our end?
Try adding these options to the link ...
-u _primary_loader-u _boot_main
I suspect the linker sees that there are no references to these symbols. Even though those symbols are defined in sections from the file booting.obj, because there are no references, the linker leaves those sections out. Using -u forces the linker to refer to those symbols, and thus keep those sections.
At this point, I'm not sure why the linker is acting this way. I think this will fix it. Then we can figure out why.
Thanks and regards,
-George
TI C/C++ Compiler Forum ModeratorPlease click Verify Answer on the best reply to your question.The Compiler Wiki answers most common questions.Track an issue with SDOWP. Enter your bug id in the "Find Record ID" box.
First of all, thank you for keep helping me with this issue.
I've tried to verify required sections presence in the object file. They are present.
Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 1 $build.attributes 0x00000000 0x00000000 0x2a 1 N 2 .text 0x00000000 0x00000000 0x0 1 Y 3 .data 0x00000000 0x00000000 0x0 1 Y 4 .bss 0x00000000 0x00000000 0x0 1 Y 5 .debug_info 0x00000000 0x00000000 0xa73 1 N 6 .booting 0x00000000 0x00000000 0x80 32 Y 7 .init_booting 0x00000000 0x00000000 0x80 32 Y 8 .debug_frame 0x00000000 0x00000000 0x27b 1 N 9 .debug_line 0x00000000 0x00000000 0xc9 1 N 10 .debug_abbrev 0x00000000 0x00000000 0xc4 1 N
Then I tried to add -u option to the linker. I attach archive with map file. Better, but not perfect. I don't understand the output clearly, but seems that there is some overlap 0x00. I am doing this with CGT 7.3.5 on CCS5.1. Unfortunately, I cannot compare with CCS3.3 and CGT 6.1.x because of another issue.
As to complete project, I would refrain from publishing it on the web, but I will try to create stripped test project just to illustrate the phenomenon. If we can proceed without it, it would save me some time.
And again, thank you for support.
rrlagicThen I tried to add -u option to the linker. I attach archive with map file. Better, but not perfect. I don't understand the output clearly, but seems that there is some overlap 0x00
OK, so now you do get the .init_booting and .booting sections in the map file. Thanks to George for suggesting the -u option.
The overlap is fine because the .vers and $BRID are marked as COPY sections. A COPY section is not actually loaded to the target memory, so it won't really overlay anything. More info on COPY sections and other special sections is here: http://processors.wiki.ti.com/index.php/Linker_Special_Section_Types
AartiG,
You think the issue is resolved? I am using out file to make hex, then bin, burned to the flash. Will check it next week.
And if possible I'd like to find the root cause,why linker was omitting those section. Is -u the only way to get it fixed?
rrlagic You think the issue is resolved? I am using out file to make hex, then bin, burned to the flash. Will check it next week. And if possible I'd like to find the root cause,why linker was omitting those section. Is -u the only way to get it fixed?
Please let us know when you've had a chance to test out the binary.
Regarding why the linker was removing those sections, we would really need a test case to analyze it further. If you're concerned about posting the complete project here on the forums, you can share it with us privately. Alternately if you can create a stripped down version that demonstrates the problem, that would also work. Please let us know if you'd like to move ahead with either of these options.
Hello AartiG,
I cannot prove binary right now as my unit has hardware problem and now passed to hardware engineer for repair, but definitely I will try and report here.
Definitely, I'd like to find the root cause of linker behaviour and willing to provide required info. As to test case, I'd like to share stripped version but still privately. Please let me know how should I do that.
Thank you for support.
rrlagicAs to test case, I'd like to share stripped version but still privately. Please let me know how should I do that.
I sent you a friend request. When you accept you can start a private conversation with me and attach a zip file with the complete project. Please also include any specific directions/instructions that may be required to reproduce the issue.
I got spare unit and tested binary. Works for me. Thus, -u option helped to keep boot sections, and there is no trouble with COPY section overlap.
Nevertheless, I'd like to continue study of the case until root cause or recommended practice would be found.
For now thanks to participants for your efforts.