--entry_point=__start
in the linker command file. But the warning
warning: entry-point symbol other than "_c_int00" specified: "__start"
is disturbing in a "no warning" environment.
So how do I suppress this warning?
TIA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
--entry_point=__start
warning: entry-point symbol other than "_c_int00" specified: "__start"
TIA
You can use diagnostic options with the linker similar to what is used with the compiler. For example, --display_error_number will show the diagnostic number for the warning, and then you can use --diag_suppress=id where id is that diagnostic number.
The options are documented in the Assembly Language Tools Users Guides: http://processors.wiki.ti.com/index.php/TI_Compiler_Information#Compiler_Manuals
Add --display_error_number to your linker options. Then build the same as before. The same diagnostics are issued, but now an ID number is present. Record that ID number. Then add the option --diag_suppress=ID to your linker options. That causes the diagnostic to not be issued.
Thanks and regards,
-George