I am trying to code with TMS320F28035 and fit a some chunk of code there. It gives me some errors, here is the main one I believe:
1. #10099-D - In advice :
"./lnk.cmd", line 48: error #10099-D: program will not fit into available memory. placement with alignment fails for section ".text" size 0x2b12 . Available memory ranges: FLASH size: 0x1000 unused: 0xe56 max hole: 0xe56
Is it related to the code size? I looked at the .map file(attached in .pdf and .docx file) and saw that under section allocation map, there is such a line :
.switch 0 00000000 00000080 FAILED TO ALLOCATE
I am not quite sure what does this supposed to mean? Any kind of explanation or suggestion is appreciated,
Regards!!
1663.TMS320C2000 Linker PC v6.docx
0363.TMS320C2000 Linker PC v6.pdf