Hi,
The following is a portion of my assembly code:
.asg B16, B16_12
.asg B17, B17_34
.asg B18, B18_56
.asg B19, B19_78
.asg B20, B20_11
.asg B21, B21_11
.asg B22, B22_11
.asg B23, B23_11
......
DDOTP4H .M2 B19_78:B18_56:B17_34:B16_12, B23_11:B22_11:B21_11:B20_11, B27_d2:B26_d1
......
But "Assembly Error" says:
Unexpected trailing operand(s) DDOTP4H .M2 B19_78:B18_56:B17_34:B16_12, B23_11:B22_11:B21_11:B20_11, B27_d2:B26_d1
After symbol substitution the line became: DDOTP4H .M2 B19_78B18B17_34:B16_12, B23_11B22B21_11:B20_11, B27_d2:B26_d1
Why?
My environment is C6678 simulator on CCS 5.4.
Is there any problem in this code, or it's a bug of Assembler?
Thanks!