When is TI's 28xx compiler going to support interfacing between C/C++ variables and symbolic quantities in inline assembly code? At present there is no such support. I can add a few lines of inline assembly, but there's no way to access any program variables unless they are static variables.
(This was one of the recommended approaches in a question I asked on stackoverflow, and someone commented this was a "MAJOR FAIL" for the compiler.)
Microchip's C compiler supports this (see their C30 compiler user's guide DS51284F, chapter 8: http://ww1.microchip.com/downloads/en/DeviceDoc/MPLAB%20C30%20UG_DS-51284f.pdf ). TI has an otherwise excellent C/C++ development environment but this seems to be a sorely missing feature, especially for small bits of assembly (5-10 instructions) that would speed up small calculations (e.g. minimum-of-3-16bit-numbers) using inline assembly w/o having to have the overhead of a function call.