Hi,
I am porting IAR Embedded workbench project source code to Code composer studio.5.5.0
The source code is building fine with IAR Embedded workbench IDE.MCU is msp430f2410.
I have created a project in CCS with the same MCU as target and i integrated all source files to the project.
During Build i have Build errors..
====================================
1) #102 "BYTE" has already been declared in the current scope tick.c line 95 C/C++ Problem
====================================
Below code exist on the Build error line for the above.
====================================
1) static volatile __no_init BYTE CurrentMode; tick.c line 95
====================================
If __no_init is removed the build error is gone. I think this IAR specific code but i need the equivalent of this in CCS?