I am getting the below warning in ccs.
=====================
Warning: #10247-D creating output section "BSLSKEY" without a SECTIONS specification.
=====================
In the linker command file, BSKSKEY section is added as below.
==========
In lnk_msp430f2410.cmd file
==========
MEMORY
{
..
BSLSKEY : origin = 0xFFDA, length = 0x0002
..
}
SECTIONS
{
..
..
}
In Application BSKSKEY is used as below.
=============
In Application code src.c
=============
#pragma RETAIN(bslkey)
#pragma DATA_SECTION(bslkey, "BSLSKEY")
const WORD bslkey = 0xAA55;
-------------------------------------------------
CCS_V5.5.0
Target MCU: MSP430F2410
Do i need to add "SECTIONS" of linker file with BSLSKEY something like below
.bslkey : {} > BSLSKEY
How can i fix this warning?