Hello,
I am working on CCS5 with a particular architecture: I have a first static library, on which is based a second static library, and finaly my executable project based on the second library.
The problem is that the two static libraries create their own .lib file, and i have to include both into my project linker to make it build.
Is there a way to include the first library into the .lib of the second one?
The goal is to have only one .lib included in my project linker.
Thanks in advance
Antoine