Hi,
I am facing problems in using _cmpyr1, _shl2 intrinsics for 6614 EVM. I included c6x.h header file in my project where prototype of these intrinsics defined but I see prototyes of these intrinsics are not included as they are #defined for TMS320C6400, TMS320C6740, TMS320C6600, TI_C6X_TESLA. I tried selecting any one of these devices but none of them are showing under the C6000 family while creating the new project. In C66xx data manual it is mentioned that these intrinsics are compatible with all C66xx devices. If I build my project with calls to these intrinsics included, compiler is not giving any error but if I run the code it is not giving proper result. Can you please help me in resolving this issue?
Thanks & Regards,
Anjibabu