Hello everybody ,
please I am using STRUCT like this for example
signed int typedef struct
{
signed int op3;
signed int op4;
signed int op5;
is there a way to force the linker to give you a complete MAP file with all the elemet position in memory ?
I mean Op2 address , Op3 address and so on .
as for now I can see the startinng address of the STRUCT but not every single element and I have to do offset calculation if not connectd via emulator .
reason behind is to provide customer maintenance people with a comeplete map file so they can ask the uC via a serial link and low level proprietary sw variable st a certain location without doing address calculation
thank you
bye
Carlo