Hi all,
I'm having trouble generating compact code using CCS5.5 vs CCS2.2 The attached file details the issue.
CCS 2.2 generates a 6 cycle loop for C671x
line 2609 of CCS2.2 of .lst file is the start of loop at line 998 that iterates with a 6 cycle kernel in attached .zip file.
CCS 5.5 generates an 18 cycle loop for C674x
line 6242 of CCS5.5 section of .lst file is the start of loop at line 998 that iterates with an 18 cycle kernel in attached .zip file.
what gives?
Also some loop code is repeated in the CCS5.5 section. There are 2 code sections that implement looping for line 998 of C source. Why is that.
Any insights appreciated.
Thanks,
Andrew