I am searching for a method of compiling 64x+ code without an installation of CCS. I have an automated build machine that needs to be able to compile projects that were developed using different versions of the Compiler, Code Generation Tools and DSP-BIOS. I would like to develop a command line mechanism to invoke a specific compiler/linker and generate the same image that CCS would have, without having to maintain a CCS installation.
Is this possible, and if so is there an example script and documentation to get me started?