Hi,
I write a firmware for an AM335x processor using TI ARM CGT V5.0.5.
In my linker command file I have something like:
// Spezielle Sektion für init.obj (Einsprung aus Second Level Bootloader) .init : { init.obj (.text) } LOAD > 0x80000000
Unfortunately I use lwIP TCP/IP stack that has a file called "init.c". Result: I have one file "init.asm" (my own file) and one file "init.c" (lwIP stack) that results in two files with identical names "init.obj". Is there a definition which obj file the linker uses for the mapping showed above?
Thanks
Patrick