Hi,
CCS Studio V5.5.00077 shows a "Syntax error" (question mark on the side and orange underlined, please see picture below) on the following line in a header file:
extern u8_t memp_memory_PBUF_POOL_base[] __attribute__((aligned(SOC_CACHELINE_SIZE_MAX)));
Strange thing is, the code builds without a problem. No error message building the code. GCC extension support is enabled in the ARM compiler options. We use V5.0.5 Code Generation Tools from TI.
I can not see any problem with this code line. Does an expert from TI has an idea?
Thanks and best regards,
Patrick