Hi I am facing a problem once i integrate the example emace code of c6xx processor to my c/c++ code , the received packet is not showing the correct data while when i run independent example code i was able to get the data correctly from a PC connected to it. the HW inturrepts are coming for a rx events but data seems to be not in correct from with a c++ integrated project.
So what could be the issues causing the Received data is not in proper valuses