Hallo
I am using C6416T.I bulid a library in C6416T. My library was bulit using CCS v3.1.19.0 and c6000 Code Generation Tools 5.1.
Is my library running in CCS v3.3 correct?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
a a96 said:Is my library running in CCS v3.3 correct?
I think you are asking whether the library you built with the version 5.1 compiler is compatible with whatever compiler version you use in CCS 3.3. I cannot give you an ironclad guarantee, but your chances are very good.
An additional comment ... All of the tools you are using are very old. The version 5.1 compiler is over 7 years old.
Thanks and regards,
-George