I want to remove the libc from my C6747 project (such as <stdio.h>, <stdlib.h> etc) because I found libc is a little bit heavier (about 100KB). In addition, libc will introduce labels with same name in the disassemble code, which should be prohibited in my project for some special reasons. However I still need some trigonometric functions like sin(), cos() and tan(). These functions are originally provided by the <math.h> in libc. How can I still use the efficient triangular functions without using the entire libc library?