Hello:
I am still not very familar with the "directive" in assembly language.
Here in the snapshot, I want to allocate 10 16-bit numbers into the directive name ".mydata".
I have two questions:
1-The ".short" is also called "directive" which reserves 16-bits of memory initialized to a value. That means if I want to put 10 16-bit digits into the directive ".mydata", I need to add ".short" to the front of every digital?
Why we need multiple directive names?
2-Why the ".mydata" cannot be put at the first column from the left? I tried to put it on the left most, but the error occured.
Thank you